Additional Uplink parameters are described in Cell Parameters (Advanced LTE FDD Uplink), PUCCH Common (Advanced LTE FDD Uplink), and Sounding Reference (Advanced LTE FDD Uplink).
|
2. PUSCH Common |
|---|
Choice: Off | On
Default Off
Double-click or use the drop-down menu to turn automatic calculation of per-slot parameters on or off.
To enable manual input for the following parameters, set to:
for slot 0/1, for slot 0/1, and for slot 0/1in the UL-SCH Tx Sequence window.
To enable manual input for the following parameters, set to:
, , (described below)
in the Cell Parameters section of the Uplink node.
Range: 0 to (Maximum resource element -1)
Default: 0
When is turned , you can enter a value for PUSCH nDMRS(1). This value is used to calculate the Cyclic Shift Alpha (see 3GPP TS36.211).
Range: 0 to 29
Default: 0
When is turned , you can enter a value for PUSCH Delta SS. This value is used to calculate the Cyclic Shift Alpha (see 3GPP TS36.211).
Choice: Inter-Subframe | Intra and Inter-Subframe
Default: Intra and Inter-Subframe
Displays the PUSCH frequency hopping mode (see 3GPP TS36.211).
Range: 0 to Maximum resource blocks
Default: 0
Displays the PUSCH Frequency Hopping Offset value (see 3GPP TS36.211).
Range: 1 to 4
Default: 1
Displays the number of sub-bands (Nsb) (see 3GPP TS36.211).
Choice: Off | On
Default Off
Double-click or use the drop-down menu to turn Supporting 64QAM on or off.
If this parameter is set to on, 64QAM modulation is available to transmit. Otherwise only QPSK and 16QAM modulation are available.
The parameter 64QAM and its maximum number of transmitted bits for a UL-SCH transport block is shown in the table below.
|
UE Category |
Maximum number of bits of an UL-SCH transport block transmitted within a TTI |
Support for 64QAM in UL |
|---|---|---|
|
Category 1 |
5160 |
No |
|
Category 2 |
25456 |
No |
|
Category 3 |
51024 |
No |
|
Category 4 |
51024 |
No |
|
Category 5 |
75376 |
Yes |